Lubrication-free bearings reduce costs in frying oil filtration equipment

Plain bearings in the filtration device increase the quality of frying oil and work even with hot vapours

Lubricant-free bearings of the stirring unit

In case of a direct contact between bearings and the product to be processed or packed, like in the case of VITO when mounting the stirring unit, the demand for an FDA approved material certainly determines the choice of the bearing. The materials used in the iglidur® A180, A200 or A500 series are suitable for the required temperatures respectively.

Profile

  • What was needed: iglidur plain bearings
  • Requirements: All components used are subject to the most stringent requirements with regard to high temperatures and aggressive cleaning agents.
  • Industry: Food industry
  • Success for the customer: Bearings made of the high-performance material iglidur A500 work reliably even under the use of hot steam and cleaning acids.
drylin filtration unit

Problem

Food safety is high on the list of priorities in Europe. In the case of frying oil, devices such as the VITO filtration device from SYS Systemfiltration GmbH are used here. As the name already suggests, the particularly compact and mobile VITO device is a system for cleaning frying oil easily and efficiently, thus at least doubling the service life.
All the components used have to meet the highest standards, not only with regard to the high temperatures prevailing there, but also sometimes due to aggressive cleaning agents. A suitable material had to be found for the bearing of the rotor of the filtration device that could meet these requirements.

Solution

For the bearings of the rotor, the choice finally fell on plain bearings made of the high-performance material iglidur A500. The bearings are located in the pump module and are directly exposed to the hot oil. Almost everywhere is cleaned with hot steam and also peracetic acids. Machine manufacturers and users from the food, filling and packaging industries therefore require resistance to such substances. In order to do justice to this claim, the values and officially confirmed plain bearing specifications stated in our product catalogue are always preceded by scientific tests with regard to durability. If there is direct contact between the plain bearing and the product to be processed or packaged, as in the case of the VITO for the bearing of the agitator, the requirement for an FDA-approved material certainly determines the selection of the bearing.

Filtration device

More on applied products here

Further interesting applications from extremely diverse areas can be found here.
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
The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "igutex", "kineKIT", "manus", "motion plastics", "pikchain", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® GmbH/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention on this website. The products offered by igus® are those of igus® GmbH