Polymer bearings replace wearing brass bearings in slurry tankers


Despite heavy soiling, the new plain bearings work in the axis system of slurry tankers.

The requirements for slurry distribution have grown enormously in the last few years. Whether cattle, pig or biogas slurry is involved, the aim is always to distribute the nutrient fertilizer evenly and economically over the agriculturally used areas without violation of the regulations governing the use of such types of fertilizer. This is where robust slurry tankers prove their worth. In their pendulum axes, lubrication-free polymer bearings withstand all adverse operating and environmental conditions when the aggressive fertilizer is being delivered.

Profile

  • What was needed: tribologically optimised iglidur® Q polymer plain bearings
  • Requirements: Heavy pollution from dirt and slurry, aggressive ammonia cloud affects all components, within the season high stress on all parts due to continuous use
  • Industry: agriculture
  • Success for the customer: The vulnerable brass bearings could be replaced by completely maintenance-free and lubrication-free iglidur plain bearings, the new bearings are robust, insensitive to dirt and dust and have a longer service life due to their low friction properties
Zunhammer slurry tanker Slurry tankers from Zunhammer GmbH distribute nutrient fertiliser evenly and economically on agricultural land. Nutrients are registered with an NIR sensor that continuously picks up information about the composition of the slurry from a slurry pipe.

Products used

Order a free sample

► iglidur plain bearings sample box

Problem

The family business Zunhammer GmbH exclusively manufactures customised agricultural vehicles. Whether tyres, distribution or docking systems, pumps or working widths - as a rule, these are customised solutions, completely from their own company. Over the year, this also includes around 450 tankers that the family business manufactures.
When a slurry tanker is planned, all components are precisely matched to each other. This applies to the tyres, the tank and the pump, but also to the chassis. Various axes systems and additional steering support options are available. For some years now, a pendular trapezoidal axis with hydraulic self-steering has been used as standard equipment in the vehicles.
Previously, brass bearings were used in the pendulum steering axes, but they had too much wear. During the transport and spreading of the slurry, the bearings were also exposed to heavy contamination and stress. Therefore, a lubricated bearing was not practical. In addition, there is always a cloud of ammonia hovering around the vehicles, which also affects all components.
As agriculture is dependent on the weather, it is not possible to drive to the field in all weathers, so a slurry tanker is only used for a maximum of 100 days a year. During this time, however, the technology must function 24 hours a day, seven days a week, without failures. There must be no technical faults whatsoever.

Solution

Four tribologically optimised iglidur Q polymer plain bearings with a diameter of 80 mm are now used in the pendulum trapezoidal axis. With polymer plain bearings made of the materials iglidur G, Q and J a suitable bearing was found for every point of the slurry tanker. Due to the freedom from maintenance and lubrication, iglidur plain bearings are very insensitive to dirt and dust. In addition, the coefficient of friction could be improved, resulting in a longer service life. 
While the wear of the brass bushings was too high, an effective and significantly more robust alternative could finally be found with the polymer bearings. The bearings in the axle do not normally come into direct contact with the slurry. But it can splash violently during distribution, so that residues are deposited that cannot be removed immediately.
And while the rotation of the steering is low, there is still a very high surface pressure. The plastic plain bearings are perfectly suited here, as they are highly abrasion-resistant under the most extreme loads and insensitive to edge loads.
Tribo-optimised polymer plain bearings made of the material "iglidur® Q" have been proving their strength in the steering arm of the tandem axle since 1996. After the lubrication-free bearings were installed, there haven't been any failures any more.

"The wear on the brass bushes was too large. Therefore, we were glad when the polymer bearings finally provided an effective alternative, because the plastic bearings are simply more robust.
 
 Sebastian Zunhammer, CEO Zunhammer GmbH
Zunhammer slurry tanker In addition to the weather, the vegetation must be suitable for spreading the slurry. For this reason, the tankers only go out on a maximum of 100 days a year. At the high season, however, they are then often on duty 24 hours a day, seven days a week.
iglidur Q polymer bearings Heavy duty polymer bearings made of iglidur Q are used in this pivoting extension arm in agricultural machinery. The lubrication-free machine components have been proving their worth for many years. With the brass bushings used in the past, the wear was too great.
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
The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "igutex", "kineKIT", "manus", "motion plastics", "pikchain", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® GmbH/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention on this website. The products offered by igus® are those of igus® GmbH