Please choose your delivery location

The selection of the country/region page can influence various factors such as price, shipping options and product availability.
My contact person
Select location

After selection of your ZIP code, we designate the relevant staff to attend to you at once.

MY(EN)

Bus cables from chainflex® are highly flexible & always guaranteed

High-Performance Bus Cables for Reliable Data Transmission in Energy Chains

In today's rapidly advancing world of automation, efficient and reliable data transmission is more critical than ever. Traditional data cables are increasingly being replaced by advanced bus systems that allow faster, more complex communication across various industrial applications. To meet the growing demand, igus® offers high-quality bus cables specifically designed for seamless data transfer in energy chains.
 
Buy bus cables

Alternate text has yet to be replaced

Ethernet

Many bus systems are based on Ethernet. Well-known brands include Profinet, CC-Link IE, EtherCat and Sercos. They are all based on a structure that has been used for many years in mainframes and PCs. Ethernet is described in categories that cover frequencies and data volume capacities from 100 Mbps to 10 Gbps. The terms CAT5, CAT5e, CAT6A and CAT7 are frequently used. These cables contain two or four pairs in a shield pair or overall shield design, depending on requirements. We have prepared an overview matrix that considers the mechanical parameters in addition to the electrical parameters just mentioned.

Here you have the opportunity to experience the CFBUS bus cable as a virtual, three-dimensional model

Bus cable CFBUS.045

Profinet

Profinet is one of the most popular bus cables for use in industry. The real-time capability option and modular concept makes it eminently well-suited to a large majority of applications. igus has nine different mechanical qualities of Profinet cable, from PVC cables to PUR cables to cables for extraordinary applications such as those involving torsional movement or requiring great strength. Profinet fits into the Industrial Ethernet standard, alongside bus systems such as Sercos, EtherCat and CC-Link IE. igus is a member of the Profinet user organisation and conforms to all required market standards.
Alternate text has yet to be replaced

Alternate text has yet to be replaced

SPE

Single Pair Ethernet (SPE), the newest addition to the group of bus systems. The new bus technology was introduced in 2019 and has since progressively conquered the market. This innovation offers new capabilities for the fast-growing IIoT market. What is special here is the cable's new design: a single pair, but still with the capability of transmitting a CAT5e signal. We are working steadily with the SPE organisation on refining and standardising this technology. This technology has notable capabilities, particularly in applications involving tight installation space.

Profibus

Today, Profibus is one of the most important industrial bus cables. It was developed in the 1990s and quickly became the standard for reliability and high data quantities. The Profinet Nutzer Organisation (PNO), Germany's Regional PI Association, is concerned with technical refinement and coordination of various member companies such as igus. The cable, with its red and green foam cores, is very distinctive. igus provides chainflex Profinet cables in PVC, PUR and TPE designs for any moving e-chain application.
Alternate text has yet to be replaced

Alternate text has yet to be replaced

CAN bus

The CAN bus is extremely tough and remarkable for its robust network protocol. Its origins are in the automotive industry, and it is commonly found in industrial systems today. The special thing about these CAN bus cables is that they are available with different cross-sections as required and are used for different applications with one or two pairs. As with other bus systems, chainflex offers cables for linear chains and for torsion.

Other bus cables

Bus cables are used in a variety of applications, and bus systems for computers or consumer electronics are also commonly used in industrial applications. One example is USB 2.0 and USB 3.0, which have distinctive connectors and can often be found in industrial cameras. The same is true for DVI, a typical monitor interface. There are also chainflex solutions for these bus cables. Some applications require prominent bus systems such as INTERBUS or DeviceNet, which are part of the CFBUS bus cable family. There is also the prominent ASi bus cable, which is easily identifiable in any system because of its yellow colour and square corners.
Alternate text has yet to be replaced

What makes a bus cable a special data cable?

While bus cables and data cables share the common function of transmitting low-energy signals, bus cables are uniquely tailored for long-term, reliable signal transmission. Unlike standard data cables, bus cables are electrically designed to align specifically with the bus system they serve. This results in different electrical properties, core cross-sections, and color codes. In essence, a bus cable is a specialized type of data cable engineered for superior signal transmission and durability in its specific application.

Expert's tip

Bus cable in motion – what is different?

When designing a bus cable, the primary focus is on ensuring reliable data transmission. The quality of data transmission is influenced by factors like the arrangement of shielding and cores, which are crucial for maintaining optimal capacitive values. However, during motion, these positional changes can affect data transmission quality. That's why our specially engineered design ensures consistent, high-quality data transmission even in motion. If uninterrupted, high-quality data transmission is vital for your operations or if you've encountered challenges in this area, we're here to help. Feel free to contact us via email for personalized support.
Expert tip

Haven't found the right one yet?


Are you familiar with our online tools?

Simply find and choose a suitable type, calculate its service life, and order it online
 
Product finder

Product finder

Get to just the right cable quickly
Service life calculator

Service life calculator

Calculate the service life of any chainflex cable
Copper surcharge calculator

Copper surcharge calculator

Calculate the current copper surcharge
chainflex configurators

Configurator for special cables

Configure your individual cable in just three minutes

e-chain

Are you still looking for an energy chain for your cable?

readychain

... or everything already harnessed?

... preferably with integrated condition monitoring?



Consulting

I look forward to answering your questions

Photo
Luther Tan

Product Manager for chainflex® cables ASEAN

Write e-mail

Shipping and consultation

In person:

Monday to Friday from 8:30 am - 5:30 pm.

Online:

24h


The terms "Apiro", "AutoChain", "CFRIP", "chainflex", "chainge", "chains for cranes", "ConProtect", "cradle-chain", "CTD", "drygear", "drylin", "dryspin", "dry-tech", "dryway", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-loop", "energy chain", "energy chain systems", "enjoyneering", "e-skin", "e-spool", "fixflex", "flizz", "i.Cee", "ibow", "igear", "iglidur", "igubal", "igumid", "igus", "igus improves what moves", "igus:bike", "igusGO", "igutex", "iguverse", "iguversum", "kineKIT", "kopla", "manus", "motion plastics", "motion polymers", "motionary", "plastics for longer life", "print2mold", "Rawbot", "RBTX", "RCYL", "readycable", "readychain", "ReBeL", "ReCyycle", "reguse", "robolink", "Rohbot", "savfe", "speedigus", "superwise", "take the dryway", "tribofilament", "tribotape", "triflex", "twisterchain", "when it moves, igus improves", "xirodur", "xiros" and "yes" are legally protected trademarks of the igus® SE & Co. KG/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries. This is a non-exhaustive list of trademarks (e.g. pending trademark applications or registered trademarks) of igus SE & Co. KG or affiliated companies of igus in Germany, the European Union, the USA and/or other countries or jurisdictions.

igus® SE & Co. KG points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention on this website. The products offered by igus® are those of igus® SE & Co. KG